cancel
Showing results for 
Search instead for 
Did you mean: 

Connect to WPA2 network using micropython

Mark Wagoner
Associate
Posted on September 28, 2017 at 18:42

I'm a noob and I actually have two problems.

First, I'm trying to connect a SPWF04SA board to a WPA2 protected network using micropython. From some examples I have found on the micropython website it looks like I should be able to use the statement:

wlan.connect('PE9000',(WLAN.WPA2,'xxxx'))

But I get the error:

Traceback (most recent call last):

File '<stdin>', line 1, in <module>

AttributeError: type object 'WLAN' has no attribute 'WPA2'

How do I specify WPA2 security when trying to connect?

My second problem is probably my own doing. After playing with the board for a while it started acting a little flaky so I tried resetting it with the command AT&F. Now, however, I can no longer start the python shell. I get the error:

ERROR:16:Cannot switch to Python shell

I have tried re-enabling the console with AT+S.SCFG=console_enabled,2 but it still doesn't work. How do I get this working again? Note the board came 'python enabled' and I haven't changed any of the jumper settings.

Thanks for any help.

#wpa2 #micropython
0 REPLIES 0