2020-01-25 7:08 PM
i got confused about STM32H745I-DISCO & some nucleo board mentioning 'mbed compliant' if i ca used with it mbed & mbed-linux os, i'm getting STM32H745I-DISCO anyways to start with - it's my first ever embedded experience but i am interested in arm mbed and want to know if i can use it with this board
2020-01-25 9:44 PM
Wow, first ever embedded experience and straight onto a dual core. For arm mbed I suggest you go to the website and look which boards are supported.
2020-01-25 11:15 PM
i am stepping in wrong maybe, but i thought it's easier to start with a such thing .. i am focusing on programming and from what i understand that one can work on a part of the system at the start and not necessary to dive into everything .. for example if it has a user led i can work on making it bilk for example
my question was because i got confused, there are some nucleo boards that are or have a lable 'arm mbed enabled or compliant' but are not on the arm mbed platforms page .. for this i am asking about this board if it's possible or can be used with arm mbed
i've choosen this so that i start with it and get matured with the same thing
2020-01-25 11:26 PM
2020-01-26 3:49 PM
thanks you hansd56, i'll start with NUCLEO-L476RG + a 16x2 display for few monthes