2023-10-11 06:26 AM
Hello,
I want to change the MCU STM32F779AIY to STM32F779NIH6
I already checked the pinout in CubeMX and i can use the same config for the peripherals at the same naming of pins (PB1, PA4 and so on).
Do i need to change anything at the software if i change the MCU?
As i can see so far, the software does not detect the type of the MCU, as long as GPIO stuff is the same (which is) it will work. Am i right here?
Thank you.
Solved! Go to Solution.
2023-10-11 06:30 AM
Correct, for this swap you won't have to change the code at all. They are effectively the same exact chip in a different package.
2023-10-11 06:30 AM
Correct, for this swap you won't have to change the code at all. They are effectively the same exact chip in a different package.