2008-05-27 12:33 PM
command line boot loader utility available?
2011-05-17 03:22 AM
great dale your util works !!!
I am quite happy for it, you should sell it to ST :) it is much better than the flashloader. oh man we are fooling arround with bin files hex files adding applications and bootloaders and then finding out how to JTAG program our boards in production, nothing works except your tool. we really need a bin file to hex file util that will handle the offsets correctly and output in right hex file format so the JTAG programmers will be happy, we use Rlink2011-05-17 03:22 AM
Hi tta,
Refer to thsi post . ST is releasing soon an official and enhanced Command line utility with the Flash Loader GUI. Cheers, STOne-32.2011-05-17 03:22 AM
> we really need a bin file to hex file util that will handle the offsets correctly
maybe ''srecord'' works for you.