2020-02-12 10:52 PM
Dear all,
The MCU : STM32F051R8T on Discovery Board
Issue : USART1 and USART2 are required. The clock of USART1 can be configured by CubeMX. However, it is not possible for that of USART2
Details
This creates big confusion.
I welcome any approximation, or explanation.
Thanks for help in advance!
Best regards!
2020-02-13 4:29 AM
> No clock MUX for USART2 in F051, but, USART2 is there. So, which clock does it use?
PCLK, i.e. APB clock.
> Both F070 and F072 have USART2. The latter has dedicated Mux, but, former[ not]
Accept it as a fact.
Note, that 'F0x0 have a separate RM, RM0360; whereas the non-zero-ending parts have RM0091.
JW
2020-02-16 11:49 PM
Thanks for the reply!