Clarification about connecting UART and SPI to the STMod+
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-10-17 8:56 AM
I am trying to connect an SPI communication device and a UART communication device to my STM32H7B3I-DK using the STMod+. From the datasheet for the discovery board, SPI and UART use the same lines (pin numbers 3 and 4) to connect the connections on the STMod+ to the discovery board. But then after reading the datasheet for the STMod+, it says that pins 2 and 8, and pins 3 and 9 are the same? This is where I'm a bit confused. So here are my questions:
- If I want enable SPI2 only or UART2 only, do I just set this by disabling the one that I don't need in ST32MXCUBE?
- If I want to use both SPI2 and UART2, do I connect the UART device to 2 and 3 and use pins 8 and 9 for the SPI device?
- Do I assume that the UART for the connector esp-01 (CN4) and the connector CN10 on the STMod+ are the same so I can only use one of them at any moment?
I have attached screenshots of the datasheets I'm referring to below. Thank you very much for your help!
Solved! Go to Solution.
- Labels:
-
SPI
-
STM32CubeMX
-
STM32H7 Series
-
UART-USART
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-10-17 9:43 AM
The STMod+ pin 1..4 are the prime pins for Usart xor SPI interfaces. Optionally, if the mcu allows and if only simple 2 wire uart is used, uart and spi can be formed with rx tx using pin 2 and 3, while SPI are using pin 1, 4, 8 and 9. The mcu can output the same peripheral signals on different pins. The I2C bus using pin 7 and 10. The connector is 2mm pitch simple mix of PMOD, Click and Seed grove connectors which extend the ecosystem from Arduino on the Fan out board.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-10-17 9:43 AM
The STMod+ pin 1..4 are the prime pins for Usart xor SPI interfaces. Optionally, if the mcu allows and if only simple 2 wire uart is used, uart and spi can be formed with rx tx using pin 2 and 3, while SPI are using pin 1, 4, 8 and 9. The mcu can output the same peripheral signals on different pins. The I2C bus using pin 7 and 10. The connector is 2mm pitch simple mix of PMOD, Click and Seed grove connectors which extend the ecosystem from Arduino on the Fan out board.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-10-17 9:45 AM
Also some newer gen usart IP have RX TX swap functions.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-10-18 12:34 AM
I see. Thank you for your clarification!