2020-09-28 12:34 AM
I wonder How Ican change the init value of the spi crc. the only thing I can see that I´m able to configure is
SPI_HandleTypeDef *pSpiHandle;
pSpiHandle->Init.CRCCalculation = SPI_CRCCALCULATION_ENABLE;
pSpiHandle->Init.CRCLength = SPI_CRC_LENGTH_16BIT;
pSpiHandle->Init.CRCPolynomial = 0x1021;using the HAL library..
But I want CCITT-FALSE and not CCITT-Zero
How can I change this?
2020-09-28 2:24 AM
I don't know what is CCITT-FALSE exactly, but the reset value of CRC->DR is fixed to 0xFFFFFFFF so after CRC reset you might need to write a value which results in the required initial value in CRC->DR.
https://community.st.com/s/question/0D50X00009XkbxTSAR/crc-calculation-unit-initialize
JW