2013-08-26 1:06 PM
While dumping some memory from the CCM on an STM32F405 at address 0x1000 FF00 I noticed the GDB memory browser window cut off at 0x1000 FFEF as the end of valid memory. The last 16 bytes of CCM didn't show. Has anyone else seen this?
I use a Segger J-Link, GDB and Eclipse. The J-Link is a few weeks behind on updates, GDB 7.2.50.20100908. Jack Peacock #ccm-gdb2013-08-26 1:48 PM
I've certainly observed boundary issues, in other debuggers, where the block it's trying to read spans the end so the whole read fails, they are typically not reading a byte at a time. In these case one parks the view window so it doesn't exceed the allowed scope.