cancel
Showing results for 
Search instead for 
Did you mean: 

Capacitor C124 on STM3221G-EVAL

eduardo2
Associate II
Posted on August 11, 2014 at 15:32

Hi:

Capacitor C124 on STM32 20-21-45-46 G-EVAL is not installed. This capacitor is part of the debounce circuitry for WAKEUP button. There are 2 more button that have the capacitor installed, so I don't understand why there's not cap on the WAKEUP button circuitry.

On the schematic (pag 54 on UM1065) says '' C124 do not fit''. I am confuse by the instruction , I don't know if  I can install the capacitor or not, can I?

I am having issues with this button, and I think is because there is not debounce for that particular switch.

#stm3221g-eval #wakeup #c124
1 REPLY 1
Posted on August 11, 2014 at 16:30

No Fit is a production/BOM instruction, not a preclusion from you adding it if you feel that's appropriate to your circuit design.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..