2018-02-12 06:54 AM
Hello,
I'm having troubles installing STM32Cube Programmer under MAC - High Sierra, recently formatted.
The installation process starts regularly and then freezes forever!
Can anyone help me??
Regards :)
2018-03-08 01:11 AM
Hi Giulio,
Can you please give us your java version ? java -version and please indicate in which step you are observing the freeze.
Best regards,
Aymen.
2018-03-08 12:03 PM
Ciao Aymen,
Thanks for your reply!!
Here's the output of the query.
java version ''9.0.1''
Java(TM) SE Runtime Environment (build 9.0.1+11)
Java HotSpot(TM) 64-Bit Server VM (build 9.0.1+11, mixed mode).
The installation freezes at the very beginning.
Thanks in advance for your support:-)
2018-03-08 11:37 PM
Hi Giulio,
Java9 is not yet supported by MAC installer. You have to install java8 if you want to use STM32CubeProgrammer.
Best Regards,
Ayman.