cancel
Showing results for 
Search instead for 
Did you mean: 

Can the STM32L073VB be used for RS-232 communication with HSI RC internal clock source (without a crystal )with an accuracy less than the accuracy listed in the EIA RS232 standard?

SPATI.1
Associate
 
1 REPLY 1
TDK
Guru

The accuracy of the HSI48 is listed in the datasheet.

https://www.st.com/resource/en/datasheet/stm32l073v8.pdf

0693W00000FCOBHQA5.png 

I doubt that ±4% accuracy is sufficient.

If you feel a post has answered your question, please click "Accept as Solution".