cancel
Showing results for 
Search instead for 
Did you mean: 

Can the ST10 DSP library be used with a STM32L4 MCU?

MCrew.1
Associate III

Looking to create a digital bandpass filter using the STM32L4 MCU and wondering if the ST10 DSP library can be used to do this?

1 ACCEPTED SOLUTION

Accepted Solutions
Ozone
Lead III

If the library is available in source code, you might try to recompile it for the STM32.

The ST10 is a totally different architecture, the link library is useless for the STM32L4.

View solution in original post

1 REPLY 1
Ozone
Lead III

If the library is available in source code, you might try to recompile it for the STM32.

The ST10 is a totally different architecture, the link library is useless for the STM32L4.