2025-05-07 5:53 AM
Hi,
I am trying to do this tutorial: https://community.st.com/t5/stm32-mcus/how-to-implement-the-usb-device-composite-class-in-stm32-using/ta-p/645017 but I can't find Azure RTOS in Middleware and software Packs. I have already downloaded the packs for azure H7 and placeit here ( C:\Users\XXXXX\STM32Cube\Repository\Packs\STMicroelectronics) but nothing in CudeIDE.
Is enybody have an idea how I can do
?
Thanks,
G.
2025-05-07 5:56 AM - edited 2025-05-07 5:56 AM
It can be found within the "Software Packs" tab.
2025-05-07 5:59 AM
I have only this...
And I can't open Manage software packs.
2025-05-07 6:34 AM
Are you using STM32CubeMX or STM32CubeIDE? And what version? Make sure it's updated.
2025-05-07 6:51 AM
I am using CubeIDE version 1.13.2 and I can't upgrade to an other version because of the firewall.
Is my path to the folder is correct ?
In Repository:
/Packs/STMicroelectronics
For information I manually create the path.
2025-05-07 8:09 AM
I'm not sure manually copying the files is having the same effect as installing them via the program.
I would guess upgrading the version would solve these issues.