2016-06-17 05:45 AM
Hi, I'm facing problem with one of St's example, this one
. I'm trying to build the SensorDemo_DMA_LowPOwer for STM32F401RE-Nucleo with the 1.8 version of system workbench for STM32. When I try to build it, I always have warning/error about unknows directory/file : Invalid project path: Referenced project is not accessible. But when I check the console, the directory and file name are correct. By the way the Readme claims that the project has been successfully tested with Version 1.8.0. Can somebody test to build this project ? Or if anyone has already worked on this project can he/she tells me if there was a particular thing to do to make it work ? Thank you.2016-06-23 05:28 AM
Hi Quentin,
Thanks for highlighting this issue,I'll report it to our team for checking.-Syrine-