cancel
Showing results for 
Search instead for 
Did you mean: 

Can't Boot after changing from STM32F401RBT6 to STM32F401RET6

mendez
Associate II

Hello,

After changing from STM32F401RBT6 to STM32F401RET6, I can no longer put the chip in boot mode. All I did was to replace the chip; my understanding is that both chips are identical except memory. Does it need additional changes?

Thanks for the help!

4 REPLIES 4
SofLit
ST Employee

Hello,

Both chips have the same boot. Only Flash and RAM sizes are different.

SofLit_0-1732197894910.png

SofLit_1-1732197925930.png

As you replaced the chip check your PCB soldering.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Yeah that is what I have been focusing; I read the AN2606 and everything is identical. Thanks again!

SofLit
ST Employee

Meanwhile you need to check the AN2606 "STM32 microcontroller system memory boot mode"

Sections:

30 STM32F401xB(C) devices

31 STM32F401xD(E) devices

What interface you are using for bootloader?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
Ozone
Lead II

>  All I did was to replace the chip; ...

What exactly you are talking about ?
Unsoldering the MCU from a board and resoldering a new one ?
Or having different PCBs populated with the RET6 instead of the RBT6 ?

Anyway, have you done something beyond visual inspection, i.e. electrical checks ?
Like comparing current consumption, checking for heated spots, etc.