cancel
Showing results for 
Search instead for 
Did you mean: 

Can't access an[y] old thread

13 REPLIES 13
TDK
Guru

I've ran into this a few times in the past week. No clue why, but Google cache has the data:

https://webcache.googleusercontent.com/search?q=cache:M7acaS0BCJkJ:https://community.st.com/s/question/0D50X00009XkhdpSAB/lowpower-management-reset+&cd=1&hl=en&ct=clnk&gl=us

If you feel a post has answered your question, please click "Accept as Solution".

Links I have to older threads don't work either, so I believe the whole shebang simply crashed and the archive is in havoc.

It's also telling how the google cache is unusable courtesy of the idiotic cookie overlay (yes I know how to bypass it thank you very much, but that's not the point).

JW

All threads older than 3 years do this. Literally - the boundary is somewhere between June and July 2018.

Given the attitude of folks who are responsible for this mess, I wouldn't be surprised if this is deliberate.

JW

TSant.2
Associate II

How to open the thread entitled "STM32F4 ADC1 starting conversion from TIM1 CC4 event - doesn't work":

https://community.st.com/s/question/0D50X00009XkZFdSAN/detail

How to bypass this cache issue more specifically?

Camilo LEMOS
Senior II

Thank you all for reporting this!

I've escalated the issue to the community IT team. I will let you know as soon as I have updates.

Apologies for the trouble.

Thanks, Camilo.

So, were you able to reproduce it?

Jan

@Community member​  Yes, I was able to reproduce it using a customer account, similar to yours. The issue doesn't happen using a moderator account, which helps us narrow down the issue a bit.

SLind.1
Associate

Same problem for me