2017-05-30 04:45 AM
Cross-post:
SW4STM32 seems to come with GCC v5
Working with exported mbed projects requires GCC v4.9.
Can the SW4STM32 be configured to use GCC v4.9 ?
If so, how?
Thanks.
#eclipse #sw4stm32-eclipse #sw4stm32 #gcc #mbed2017-05-30 06:09 AM
I see this has been marked as an 'Action Item' - what does that actually mean?
2017-05-30 09:05 AM
Hi
Neil.Andrew
,I see this has been marked as an 'Action Item' - what does that actually mean?
This means that your entry is under review.
-Nesrine-
2017-05-31 12:15 AM
Cross-post:
http://www.openstm32.org/tiki-view_forum_thread.php?forumId=7&comments_parentId=5150
- a 'hack' is noted as a workaround.But this is really a Big Issue for anyone wanting to export anything for STM32 from mbed.
2017-05-31 01:07 AM
Hi Andrew,
2 solutions were described on OpenSTM32 forum to not stay blocked with this issue
A clean way to configure the toolchain in use within the project properties and indeed another considered as a 'hack'.
The first do the job and should be acceptable while you don't have plenty of projects to configure.
2017-05-31 02:02 AM
Thanks,
ELMHIRI.Syrine
- but still unclear what that actually means.Is that for forum moderation? Or the SW4STM32 development team? Or ...
2017-06-07 11:46 AM
I tried tried setting the path in the Project Properties, and it didn't work - see the other thread.
2017-06-09 04:28 AM
Looking your System Workbench version (1.13.1) and our bugs database I confirm that the defect your are facing is fixed since 1.14.
It's time to give a chance to version 2.0 !
2017-06-09 07:44 AM
going to give v2.0 a go ...