cancel
Showing results for 
Search instead for 
Did you mean: 

Can ST Link support two differrent ports for two board simultaneously?

Vu.Andy
Associate III
Posted on June 27, 2016 at 18:06

I am planning to debug using two separate boards talking to each other.  I am using Keil uVision.  Is it possible to have Keil debugging two separate boards on the same PC? 

1 REPLY 1
Posted on June 27, 2016 at 19:06

Depends

Might depend on version of Keil, drivers, DLL and specific pods.

One of the stand-alone ST-LINK I have doesn't provide a serial#

For U-LINK you can pick individual debug pods via the the debugger settings pane, and this allow specific instances of Keil to talk to specific pods/boards

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..