2019-06-11 2:53 PM
Hello everyone !
I'm new here and i wanted to know how these lines say please??
I wanted to have microsecond delay for my ultrasonic sensor.
Thanks for all your help!
void usDelay(uint32_t uSec)
{
if(uSec < 2) uSec = 2;
usTIM->ARR = uSec - 1;
usTIM->EGR = 1;
usTIM->SR &= ~1;
usTIM->CR1 |= 1;
while((usTIM->SR&0x0001) != 1);
usTIM->SR &= ~(0x0001);
}
2019-06-11 3:08 PM
First, read the timer chapter in reference manual.
void usDelay(uint32_t uSec)
{
if(uSec < 2) uSec = 2; // sanitize input value, minimum possible duration using this method is 2usec
usTIM->ARR = uSec - 1; // counter counts up to 0 to ARR inclusive
usTIM->EGR = 1; // generate update, this ensures ARR value is copied to the "active" register even its shadowing is on
usTIM->SR &= ~1; // clear bit 0 i.e. update flag in status register - this is incorrectly written, it should be = rather than &=
usTIM->CR1 |= 1; // start counter
while((usTIM->SR&0x0001) != 1); // wait until update
usTIM->SR &= ~(0x0001); // clear update again, again incorrectly (and here, it's better to stop the counter first)
}> I wanted to have microsecond delay for my ultrasonic sensor.
There's more to that, e.g. you have to switch on optimization.
JW
2019-06-11 9:29 PM
I don't think these:
usTIM->SR &= ~1;
are wrong. At least timer 1 has a reserved bit in the status register. It shouldn't be written "1".
Then it's better not to alter the other bits.
2019-06-11 11:58 PM
https://community.st.com/s/feed/0D50X00009bLSAZSA4
(formatting and videos did not survive migration from jive)
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.