Skip to main content
RLavi
Associate
June 10, 2019
Question

Hello, Can anyone tell me STM controllers which support all the required capabilities as ADSP-CM408F Analog Devices? Thanks

  • June 10, 2019
  • 12 replies
  • 2097 views

..

    This topic has been closed for replies.

    12 replies

    Tesla DeLorean
    Guru
    June 10, 2019

    None of them

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    MikeDB
    Senior II
    June 10, 2019

    What are your actual 'required capabilities' ? I assume if you needed all of them, you would use the ADI chip

    RLavi
    RLaviAuthor
    Associate
    June 10, 2019

    Floating point operations

    16 bit ADC *2 

    UART support RS-485

    Ethernet support 

    2 DAC 12 Bit 

    Cache Memory - 128 -348K byte 

    Flash Memory – 2 * 10^6 * 8 bits

    Clock Speed is 240 MHz 

    Low, high pass filtering available

    Watchdog 

    SPI and I2C Communication Possible.

    DMA 

    MPU 

    These all I need

    MikeDB
    Senior II
    June 10, 2019

    Some of the high end processors can do most of that, but the ADC will always be the gotcha. ADI's ones are simply better.

    Load up the MCU finder and enter what you really need

    https://www.st.com/en/development-tools/st-mcu-finder.html

    RLavi
    RLaviAuthor
    Associate
    June 11, 2019

    I do not want to compromise on ADCs and Yes they have limited the support on DSPs.

    MikeDB
    Senior II
    June 11, 2019

    I'd go for an F7 part with the bits you need and an SPI A-D convertor chip then

    RLavi
    RLaviAuthor
    Associate
    June 11, 2019

    Thank you for the advice. will look into it

    MikeDB
    Senior II
    June 11, 2019

    Start on the Mouser, RS or whoever your preferred distributor is and you should find something that is simple to connect for about $2. The advantage of being off-chip is you'll actually get better resolution and a lower noise floor as well.