2021-04-06 12:34 AM
Dear Community,
can someone advice a min 8Mbit psram for the STM32F479?
I only find some who has address pins up to A20 but the uc has only up to 16 or did I missunterstand something?
best regards
Solved! Go to Solution.
2021-04-12 3:47 AM
Hello @Dany,
I suggest to look at AN4861, Table 20 "Example of graphic implantations with STM32 in different hardware configurations", for 400x600 I think at least you need LQFP144 package and with LQFP100 you should aim for low end display configuration.
For the PSRAM with STM32F479 LQFP100, you need a ADMUX Pseudo SRAM (support a multiplexed address/data bus) for example AS1C4M16PL-70BIN but with the STM32F479 LQFP100 you don't have the upper address signals available (A[21:16]), so you only have 16 address signals to work with.
To calculate the size of the memory knowing number of address lines and data width you have the formula:
Size = (2^(number of address lines)) * data width
For example, the one you attached have 19 address line and 16bit data width so:
(2^19) * 16bit = 512K * 16 = 8Mbit
and in the case of F479 LQFP100 you have:
(2^16) * 16bit = 64K * 16 = 1Mbit
Hope this help.
Regards,
Mahmoud.
2021-04-06 7:53 AM
Hello @Dany ,
Which package are you using ?
It depends on the package that you are used.
You can check the PSRAM configuration and address max with STM32CubeMX.
For example, with LQFP100 package : Max 16 bits for Muxed PSRAM.
You can refer to the Table 10. STM32F479xx pin and ball definitions in the STM32F479xx datasheet to check the PSRAM address pins.
Imen
2021-04-07 10:40 AM
Sorry - I have to use the STM32F479 in LQFP100 package but somehow I can't find any PSRAM with up 8Mbit+ which can be used.. or I missunderstand how it should work.
Hopefully you can help me to get in the rigth direction.
EDIT: Am I right that if I use this RAM I'm only able to use 128 kbyte by leaving A16-A18 unconnected / gnd?
So it looks like its not possible to drive 400 x 600 display with that package?
Thanks
2021-04-12 3:47 AM
Hello @Dany,
I suggest to look at AN4861, Table 20 "Example of graphic implantations with STM32 in different hardware configurations", for 400x600 I think at least you need LQFP144 package and with LQFP100 you should aim for low end display configuration.
For the PSRAM with STM32F479 LQFP100, you need a ADMUX Pseudo SRAM (support a multiplexed address/data bus) for example AS1C4M16PL-70BIN but with the STM32F479 LQFP100 you don't have the upper address signals available (A[21:16]), so you only have 16 address signals to work with.
To calculate the size of the memory knowing number of address lines and data width you have the formula:
Size = (2^(number of address lines)) * data width
For example, the one you attached have 19 address line and 16bit data width so:
(2^19) * 16bit = 512K * 16 = 8Mbit
and in the case of F479 LQFP100 you have:
(2^16) * 16bit = 64K * 16 = 1Mbit
Hope this help.
Regards,
Mahmoud.