2018-01-11 02:54 AM
Under Linux Debian Stretch:
- if I use the shortcut nothing happens
- if I type ./STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/STM32CubeProgrammerLauncher,
I have this error message: Error: Could not find or load main class com.st.app.Main
What should I do in order to run Cube Programmer ?
Regards
Cedric
Solved! Go to Solution.
2018-10-15 02:37 PM
Sure, I know. It uses JDK11 and JavaFX is installed. Other JavaFX applications works without any problems.
2019-01-11 07:45 AM
I have the same problem now, after upgrading to Java 11. openjfx is installed, and shows version 11. CubeProgrammer was working fine with Java 8.
Is CubeProgrammer incompatible with Java 11? :-(
2019-01-15 10:38 PM
Well, I upgraded to (K)Ubuntu 18.10 and can no longer get it to work using update-java-alternatives - even (especially?) with openjdk-11 which has openjfx installed. Tried a few things to get this going unsuccessfully: a PPA for Ubuntu that installs Oracle JDK8 - alas not functional today; also version 1.4.0 of the STMCubeProgrammer.
Interesting wrinkles are that the Trusted Package Creator launches from the shell and appears to work and appears to be using OpenJFX.
The STM32_programmer_CLI works fine on 18.10 - I just programmed a board with it.
I note with some interest in the 1.4.0 install there's a C++ library with a Qt example...
2019-01-15 11:19 PM
2019-06-22 12:22 AM
Hi,
I have some problems with launch CubeProg from Ubuntu.
$ ./STM32CubeProgrammer
/usr/local/STMicroelectronics/STM32CubeProgrammer/bin/STM32CubeProgrammerLauncher
/usr/local/STMicroelectronics/STM32CubeProgrammer/bin
JavaFX NOT installed => warn user
But openjfx installed:
$ dpkg -l | grep openjfx
ii libopenjfx-java 11.0.2+1-1~18.04.2 all JavaFX/OpenJFX - Rich client application platform for Java (Java libraries)
ii libopenjfx-jni 11.0.2+1-1~18.04.2 amd64 JavaFX/OpenJFX - Rich client application platform for Java (native libraries)
ii openjfx 11.0.2+1-1~18.04.2 amd64 JavaFX/OpenJFX - Rich client application platform for Java
ii openjfx-source 11.0.2+1-1~18.04.2 all JavaFX/OpenJFX - Rich client application platform for Java (sources)
$ update-java-alternatives -l
java-1.11.0-openjdk-amd64 1111 /usr/lib/jvm/java-1.11.0-openjdk-amd64
Please any help!
2019-06-22 01:04 AM
SOLVED.
Need doungrade jdk & jfx
# apt install apt install openjdk-8-jdk openjfx=8u161-b12-1ubuntu2 libopenjfx-java=8u161-b12-1ubuntu2 libopenjfx-jni=8u161-b12-1ubuntu2
than
# update-alternatives --config java
and set java-8-openjdk
And hold the version:
echo "openjfx hold"|dpkg --set-selections ; echo "libopenjfx-java hold"|dpkg --set-selections ; \
echo "libopenjfx-jni hold"|dpkg --set-selections ; echo "openjfx-source hold"|dpkg --set-selections
2019-07-08 12:38 PM
I received the same error message from STM32CubeProgrammer 2.0.1 after upgrading Debian 9 "Stretch" (JRE v8) to Debian 10 "Buster" (JRE v11). I attempted to downgrade back to JRE/JFX v8:
$ sudo apt install openjdk-8-jdk openjdk-8-jre openjfx=8u111-b14-1 libopenjfx-java=8u111-b14-1 libopenjfx-jni=8u111-b14-1
STM32CubeProgrammer briefly started, but then crashed:
# A fatal error has been detected by the Java Runtime Environment:
#
# SIGSEGV (0xb) at pc=0x00007ffb4b334ef8, pid=27084, tid=0x00007ffb9d9ef700
#
# JRE version: OpenJDK Runtime Environment (8.0_212-b01) (build 1.8.0_212-8u212-b01-1~deb9u1-b01)
# Java VM: OpenJDK 64-Bit Server VM (25.212-b01 mixed mode linux-amd64 compressed oops)
# Problematic frame:
# C [libjfxwebkit.so+0x1883ef8]
What worked for me was a wrapper script specifying Oracle JRE 8 64bit, as detailed in this thread:
https://community.st.com/s/question/0D50X00009q3X4jSAE/stm32cubeprogrammer-for-linux
Original script reproduced below. I downloaded jre-8u212-linux-x64.tar.gz and modified the script to suit.
#!/bin/bash
# Set path of Oracle JRE 8
JAVA_HOME=/opt/jre1.8.0_202-amd64/
PATH=$JAVA_HOME/bin/:$PATH
# Unpack libraries, if necessary
cd $JAVA_HOME/lib
if [ ! -f rt.jar ]; then
../bin/unpack200 rt.pack rt.jar
fi
if [ ! -f jsse.jar ]; then
../bin/unpack200 jsse.pack jsse.jar
fi
if [ ! -f charsets.jar ]; then
../bin/unpack200 charsets.pack charsets.jar
fi
# CHeck Java version
java -version
# Start STM32 Cube Programmer
cd /opt/STM32CubeProgrammer
bin/STM32CubeProgrammer
2019-10-22 11:59 AM
I am not able to start STM32CubeProgrammer even installed Oracle JDK 13.0.1 and openjfx:
System: Ubuntu 18.04 VirtualBox on MacOS 10.15:
jiang@Jiang-Ubuntu18:~$ STM32CubeProgrammer
Error: Could not find or load main class com.st.app.Main
Caused by: java.lang.NoClassDefFoundError: javafx/application/Application
jiang@Jiang-Ubuntu18:~$ java --version
java 13.0.1 2019-10-15
Java(TM) SE Runtime Environment (build 13.0.1+9)
Java HotSpot(TM) 64-Bit Server VM (build 13.0.1+9, mixed mode, sharing)
jiang@Jiang-Ubuntu18:~$ dpkg -l | grep openjfx
ii libopenjfx-java 11.0.2+1-1~18.04.2 all JavaFX/OpenJFX - Rich client application platform for Java (Java libraries)
ii libopenjfx-jni 11.0.2+1-1~18.04.2 amd64 JavaFX/OpenJFX - Rich client application platform for Java (native libraries)
ii openjfx 11.0.2+1-1~18.04.2 amd64 JavaFX/OpenJFX - Rich client application platform for Java
ii openjfx-source 11.0.2+1-1~18.04.2 all JavaFX/OpenJFX - Rich client application platform for Java (sources)
jiang@Jiang-Ubuntu18:~$
2019-11-04 10:22 AM
Hi guys. The same issue I have with java. Cannot download Oracle Java,OpenJDK is preferable as there are lot of software components which are developed with OpenJDK.
2019-11-25 07:36 AM
Only works with OpenJDK < v8, tested with v11 to v13, all fail to load
and with v8, get a lot of warnings
┌─┤[$]|[sl1pkn07]|[sL1pKn07]|[~/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin]|
└───╼ ./STM32CubeProgrammer
No properties file found
java.io.FileNotFoundException: /home/sl1pkn07/.STM32CubeProgrammer/config.properties (No existe el fichero o el directorio)
at java.io.FileInputStream.open0(Native Method)
at java.io.FileInputStream.open(FileInputStream.java:195)
at java.io.FileInputStream.<init>(FileInputStream.java:138)
at java.io.FileInputStream.<init>(FileInputStream.java:93)
at com.st.controllers.MainWindowController.initialize(MainWindowController.java:292)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:2548)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:2441)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:3214)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:3175)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:3148)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:3124)
at javafx.fxml.FXMLLoader.loadImpl(FXMLLoader.java:3104)
at javafx.fxml.FXMLLoader.load(FXMLLoader.java:3097)
at com.st.app.Main.start(Main.java:38)
at com.sun.javafx.application.LauncherImpl.lambda$launchApplication1$8(LauncherImpl.java:863)
at com.sun.javafx.application.PlatformImpl.lambda$runAndWait$7(PlatformImpl.java:326)
at com.sun.javafx.application.PlatformImpl.lambda$null$5(PlatformImpl.java:295)
at java.security.AccessController.doPrivileged(Native Method)
at com.sun.javafx.application.PlatformImpl.lambda$runLater$6(PlatformImpl.java:294)
at com.sun.glass.ui.InvokeLaterDispatcher$Future.run(InvokeLaterDispatcher.java:95)
at com.sun.glass.ui.gtk.GtkApplication._runLoop(Native Method)
at com.sun.glass.ui.gtk.GtkApplication.lambda$null$10(GtkApplication.java:245)
at java.lang.Thread.run(Thread.java:748)
jar:file:/home/sl1pkn07/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/STM32CubeProgrammerLauncher!/fxml/Config.fxml
java.lang.ClassNotFoundException: com.sun.deploy.uitoolkit.impl.fx.HostServicesFactory
at java.net.URLClassLoader.findClass(URLClassLoader.java:382)
at java.lang.ClassLoader.loadClass(ClassLoader.java:418)
at java.lang.ClassLoader.loadClass(ClassLoader.java:351)
at java.lang.Class.forName0(Native Method)
at java.lang.Class.forName(Class.java:348)
at com.sun.javafx.application.HostServicesDelegate.lambda$getInstance$0(HostServicesDelegate.java:52)
at java.security.AccessController.doPrivileged(Native Method)
at com.sun.javafx.application.HostServicesDelegate.getInstance(HostServicesDelegate.java:45)
at javafx.application.HostServices.<init>(HostServices.java:52)
at javafx.application.Application.getHostServices(Application.java:334)
at com.st.app.Main.start(Main.java:51)
at com.sun.javafx.application.LauncherImpl.lambda$launchApplication1$8(LauncherImpl.java:863)
at com.sun.javafx.application.PlatformImpl.lambda$runAndWait$7(PlatformImpl.java:326)
at com.sun.javafx.application.PlatformImpl.lambda$null$5(PlatformImpl.java:295)
at java.security.AccessController.doPrivileged(Native Method)
at com.sun.javafx.application.PlatformImpl.lambda$runLater$6(PlatformImpl.java:294)
at com.sun.glass.ui.InvokeLaterDispatcher$Future.run(InvokeLaterDispatcher.java:95)
at com.sun.glass.ui.gtk.GtkApplication._runLoop(Native Method)
at com.sun.glass.ui.gtk.GtkApplication.lambda$null$10(GtkApplication.java:245)
at java.lang.Thread.run(Thread.java:748)
(java:1397575): Gtk-WARNING **: 16:27:18.763: Imposible encontrar el motor de temas en la ruta al _modulo: «adwaita»,
(java:1397575): Gtk-WARNING **: 16:27:18.768: Imposible encontrar el motor de temas en la ruta al _modulo: «adwaita»,
Exception in thread "JavaFX Application Thread" java.lang.NullPointerException
at com.st.controllers.MainWindowController$1.run(MainWindowController.java:208)
at com.sun.javafx.application.PlatformImpl.lambda$null$5(PlatformImpl.java:295)
at java.security.AccessController.doPrivileged(Native Method)
at com.sun.javafx.application.PlatformImpl.lambda$runLater$6(PlatformImpl.java:294)
at com.sun.glass.ui.InvokeLaterDispatcher$Future.run(InvokeLaterDispatcher.java:95)
at com.sun.glass.ui.gtk.GtkApplication._runLoop(Native Method)
at com.sun.glass.ui.gtk.GtkApplication.lambda$null$10(GtkApplication.java:245)
at java.lang.Thread.run(Thread.java:748)
55 external Loader list
greetings