cancel
Showing results for 
Search instead for 
Did you mean: 

Can I2C master support both high speed mode and fast mode?

KDu.13
Associate

We use stm32g474re in our project. The i2c devices used in our board have two types, one support high-speed mode while the others doesnot. Currently, i set the i2c master with fast mode(400K). Is it possible to set i2c master with high-speed mode and commuicate with slave in fast mode?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Igor Cesko
ST Employee

Hi KDu.13 (Community Member),

The I2C master set to high-speed mode should communicate only with I2C slaves also set to high-speed mode. In STM32 devices we have I2C supporting Fast mode plus (FM+) mode. High-speed I2C mode is a bit different from fast mode (current source as pull-up, no clock stretching in middle, ... ).

The difference between different I2C modes can be read in a short articles:

https://www.i2c-bus.org/fast-mode-plus/

https://www.i2c-bus.org/highspeed/

https://www.i2c-bus.org/fastmode/

Regards

Igor