2023-11-08 11:15 AM - last edited on 2023-11-10 5:35 AM by Amel NASRI
I want to use STM32 PD-PHY to enable Debug Access Mode (DAM), so I need to connect both CC1 and CC2 and set different Rp values. For example apply Rp - 3A on CC1 and Rp - 1.5A on CC2.
Is it possible to do that with STM32?
If so, what family of STM32 can do that?
Thanks!
Solved! Go to Solution.
2023-11-10 12:11 AM
Hello, concerning the Debug Access Mode (DAM), this is not supported in any STM32 as of today. I believe the first ever enquiries on this feature have only come in the last weeks. Best regards, Richard
2023-11-10 12:11 AM
Hello, concerning the Debug Access Mode (DAM), this is not supported in any STM32 as of today. I believe the first ever enquiries on this feature have only come in the last weeks. Best regards, Richard