2021-04-23 4:42 PM
Hello !
Hope you're all doing well.
I have a little problem here, my CAN BUS Tx is not working on "Normal Mode"
Any idea why it behaves like this?
Thank you :D
Solved! Go to Solution.
2021-04-30 10:15 AM
In the end it was a voltage level issue with the transceiver standby pin. Every thing works fine now
2021-04-23 5:18 PM
Does it report some error or status that might be helpful in identifying the mode of failure?
Anything that will receiver and acknowledge the specific message ID being transmitted?
Is there a bus analyzer? What doesn't it see/report?
2021-04-24 9:21 AM
I have a bus analyser to receive and transmit frames and an oscilloscope to monitor the signals.
The reception works fine and the bus analyser doesn't show any error
2021-04-30 10:15 AM
In the end it was a voltage level issue with the transceiver standby pin. Every thing works fine now
2025-03-03 1:17 PM
I am also facing a similar issue, can you tell me how you resolved it?