2019-06-09 4:53 AM
Dear Members,
How can I count a pulse from a sensor with timer ?
How can I calculate the period of this pulse ?
samplebuff[i].ired = buffer_rx[ j ];
samplebuff[i].ired <<= 8U;
samplebuff[i].ired |= buffer_rx[ j + 1 ];
between
samplebuff[i].ired = buffer_rx[ j ];
and another
samplebuff[i].ired = buffer_rx[ j ];
?
Thanks
2019-06-10 3:52 AM
HAL_I2C_Master_Receive(&hi2c2, 0xAF, buffer_rx ,number_sample*4, 100); //receive 4 bytes from MAX30100
for(i=j=0;i<=number_sample;i++,j+=4)
{
samplesRecorded++;
period[i]= HAL_GetTick();
printf("========================IR RED BEGIN==========================\r\n");
samplebuff[i].ired = buffer_rx[ j ];
samplebuff[i].ired <<= 8U;
samplebuff[i].ired |= buffer_rx[ j + 1 ];
printf("Data %u ",i);
printf("Output MAX30100,0x09 register (FIFO DATA) IR : %u \r\n", samplebuff[i].ired);
dcFilterIR = dcRemoval(samplebuff[i].ired,dcFilterIR);
printf("DC filterIR = %f\r\n",dcFilterIR);
meanDiffResIR=medfilter(dcFilterIR);
printf("MeanDiff filterIR = %f\r\n",meanDiffResIR);
lowPassFilterIR = lowPassButterworthFilter(meanDiffResIR);
printf("LowPass filterIR = %f\r\n",lowPassFilterIR);
printf("Timestamp After IRRED data= %u \r\n",period[i]);
max = 0;
if ( lowPassFilterIR>max)
{
max = lowPassFilterIR;
printf("LowPassFilterIR max %f \r\n",lowPassFilterIR);
printf("Max timestamp IRRED= %u \r\n\n",period[i]);
float heartbeat = 60000 / period[0] -period[1];
printf ("Heart beat : %f \r\n",heartbeat);
}
with hal_getsystick(), I get the value, but I got negative on the heartbeat,
How can I capture maximum value time ? I don't understand.
thanks
2019-06-10 4:54 AM
You understand C comes with qsort(), right?
You need to relate the time with the samples you have. None of your code seems to account for time.
You could perhaps look at the zero crossing, Or min/max for a sinewave 1/2 frequency.
Perhaps review some texts on signal processing.
Surely App Notes and code examples exist for the MAX30100 parts?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.