2019-01-14 7:51 AM
Hello,
Do you plan to enable C++17 or gnu++17 option in the general setting panel for C++ ?
Seems like the already bundled GCC compiler support quite a few of C++17 features, and an update to latest gcc-arm would be nice too.
I'm mainly looking for chrono, std::apply, etc.
In the meantime I'll try to update it by myself (I hope it can be done).
Thomas.
2019-01-14 8:51 AM
Back,
Ok installed latest GSS-ARM version. It kinda works BUT:
All this is ok, no big deal.
More annoying is Atollic comes with CDT 9.3.0 which doesn't have support for c++17.
Updating to CDT 9.6 would add at least some (nested namespace anyone ?).
I don't think I can update CDT in Atollic on my own, can I ?
Thomas.
2019-01-14 12:15 PM
Back again,
Just for "fun" I installed barebone eclipse + CDT and a couple plugins to compile for ARM and debug with J-Link probes.
Spent some time configuring the thing, but it works not too bad, compilers gives me a sh*t ton of new warnings (including very interesting ones !!!), I can compile, flash and debug.
Except when debugging as soon as I enable ISRs step over sends me to ISR and not the next line of code.
This makes it totally useless.
So please, new version of Atollic with all good stuff you already have in it, but with updated versions of Eclipse, GCC, CDT, etc.
I wish I could update CDT on my own in Atollic ...
Let me know if you have some beta to test ;)
Thomas.
2019-01-15 12:02 AM
What "a couple plugins"? Have you tried to use the GNU MCU Eclipse?