2021-01-28 10:26 AM
Hi Al
Wondering how do you test the infrastructure before delivering it to the application teams?
I’m basically referring to the HAL layer , CMSIS and all BSP layer with peripherals.
Is there a known methodology for validation tests for these capabilities ?
Thanks!
Solved! Go to Solution.
2021-01-28 01:41 PM
Test it thoroughly so they aren't constantly calling and complaining... or when they do you know it's their fault.
Seriously, if you code functionality, be it using IRQs or DMAs, make sure it works in a couple of scenarios, both simple and stressed.
Catch dumb usage with asserts(), especially if there are known limits on memory regions or alignments.
Assume they won't check error returns, be able to instrument or assert when errors are ignored in cascade failure.
Assume callbacks and pointers will be passed as NULL
If you use malloc()/free() make sure you can detect failures there, out of memory, double free, orphans.
If you have sanity checks they'll learn not to call until those are cleared.
Test the code you write. Test the QSPI, test the serial interfaces, test they all work together.
Check every pin on the schematic, understand what kind of coverage you have, and which are most critical to the teams. If need be loop back pins / uarts and check things that would be off-board or pending other development or parts.
Have Error_Handler() and HardFault_Handler() output comprehensive information so you can immediately go to source lines in your BSP and understand what might have broken, and if a new assert is required. Be in a position to bat balls immediately back over the net, not scrabble to understand the failure each time, don't be the person to blame for holding up development. You want their manager holding their feet to the fire, not yours.
Use the slack time you now don't have to triage everything in to testing a larger number of corner cases.
Run lint or other coverage / static analysis tools on your code, find the holes before others.
2021-01-28 01:41 PM
Test it thoroughly so they aren't constantly calling and complaining... or when they do you know it's their fault.
Seriously, if you code functionality, be it using IRQs or DMAs, make sure it works in a couple of scenarios, both simple and stressed.
Catch dumb usage with asserts(), especially if there are known limits on memory regions or alignments.
Assume they won't check error returns, be able to instrument or assert when errors are ignored in cascade failure.
Assume callbacks and pointers will be passed as NULL
If you use malloc()/free() make sure you can detect failures there, out of memory, double free, orphans.
If you have sanity checks they'll learn not to call until those are cleared.
Test the code you write. Test the QSPI, test the serial interfaces, test they all work together.
Check every pin on the schematic, understand what kind of coverage you have, and which are most critical to the teams. If need be loop back pins / uarts and check things that would be off-board or pending other development or parts.
Have Error_Handler() and HardFault_Handler() output comprehensive information so you can immediately go to source lines in your BSP and understand what might have broken, and if a new assert is required. Be in a position to bat balls immediately back over the net, not scrabble to understand the failure each time, don't be the person to blame for holding up development. You want their manager holding their feet to the fire, not yours.
Use the slack time you now don't have to triage everything in to testing a larger number of corner cases.
Run lint or other coverage / static analysis tools on your code, find the holes before others.
2021-01-28 03:47 PM
My €0.02... Create your own mock-up project using most of infrastructure that you provide to the team.
This way you have a runnable code to toy with, and are independent from the real project(s).
Have a set of unit tests for all needed functions (debug prints, timers, LEDs, interrupts, memories, library functions... and yes, fault handlers).
This may need some tweaking. For example, if the "real" firmware is started by a bootloader, make sure that the same bootloader can run your test instead.
If the real hardware is in high demand (or not ready yet) but something can be tested on a cheap evaluation board - make a project for the eval board.
Good luck.
-- pa
2021-01-29 01:10 AM
Wow thanks guys for the tips.
Great to hear we all face the same challenges in this field.
Any idea about an HSID document example for STM32 MCUs or any other uC ?
My goal is to define the exact requirement between the board designer and BSP engineer.