Skip to main content
DBine.1
Visitor II
January 28, 2021
Solved

STM32H753: How is an ECC in the L1 caches reported

  • January 28, 2021
  • 1 reply
  • 942 views

Hi,

I'm currently working on a STM32H753. I'm trying to figure out how an ECC error upon a cache look up is reported. The cortex M7 reference manual doesn't provide much info in that regards with the following text:

Each cache can also be configured with ECC. If ECC is implemented and enabled, then the tags

associated with each line, and data read from the cache are checked whenever a lookup is

performed in the cache and, if possible, the data is corrected before being used in the processor.

A full description of ECC error checking and correction is beyond the scope of this document.

Contact ARM if you require more information.

I'm expecting a bus fault to be reported but I'm not able to find a documentation with that information. I'm waiting for an answer from ARM but is there anything specific to the implementation made by ST that would impact how this fault would be reported ?

Kind Regards,

David

This topic has been closed for replies.
Best answer by Amel NASRI

Hi @DBine.1​ ,

There is a dedicated application note which describes the error correction code (ECC) management and implementation on STM32H7 Series.

It is AN5342. Please let me know if this answers your request. If yes, you can select my answer as best.

If you think that there is still some more details, it will be interesting to share them with us. This will help to improve this document's document.

Amel

1 reply

Amel NASRI
Amel NASRIBest answer
ST Technical Moderator
January 29, 2021

Hi @DBine.1​ ,

There is a dedicated application note which describes the error correction code (ECC) management and implementation on STM32H7 Series.

It is AN5342. Please let me know if this answers your request. If yes, you can select my answer as best.

If you think that there is still some more details, it will be interesting to share them with us. This will help to improve this document's document.

Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.