2012-04-10 08:48 AM
Hi all,
I want to measure the brightness using a light dependent resistor ''LDR'' uisng the stm32l15x devices. I an thinking to use the ADC to measure the ldr output but the the curve of the resistance vs illumination flux shows a logarithmic function. Is there somebody who did it?Thnaks & Regards,MCU Lüfter
2012-04-11 06:48 AM
I have seen light pulses of a few microseconds length from a LED device, measured with a photo-LED as receiver. You are of course lost if you want to detect this with a LDR.
On the other hand, the LDR does the integration for you, if you don't need this fast detection. Basically I need to agree with Erik - find out what you really need.2012-04-11 07:14 AM
It's used on the STM32L152D-EVAL
See page 43 for schematichttp://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/USER_MANUAL/DM00049334.pdf
2012-04-11 07:22 AM
You haven't said what range of light intensities you wish to measure. I will assume sunlight on a photo grey card to dark.
A voltage divider with reference feeding a 100K programmable resister connected to the light sensor then to ground will work. A buffer amp will be required for the ADC signal from the resister. The programmable resister is required to get an acceptable signal over the full LDR range. Software logic will be required to hunt for an acceptable programmable resister setting. The LDR offset can be up to +/- 50%, so you will need to calibrate using a known light source. Reading a photo grey card illuminated at high noon will probably suffice. The offset can be either a trimming resister on each board, or a constant in each mcu load. If your objective is lowest cost, Erik's recommendation of an integrated and calibrated chip instead of a three or four component solution is the way to go. Cheers, Hal2012-04-11 08:20 AM
I want to use the ldr VT9ON1 and the stm32l152 device.
I want a low cost solution, with acceptable accuracy.
not that low cost, to use a LDR you need an OP-amp between the resistor and the A/D ot you will get nothing really useable. (the input leakage of a port pin is very temperature dependent combined with the high resistance of the LDR it will be very imprecise). can you live with 10% drift, tolerance, ... say so If it is that you are doing a one-off with the eval board, say so. are you aware that with the LDR it takes a minimum of 50 milliseconds to measure the light, say so ''acceptable accuracy'' is not a design criteria, be precise and say so what are you measuring daylight, TV output, ... say so Erik
2012-04-11 08:28 AM
It's used on the STM32L152D-EVAL
See page 43 for schematic
good enough for ''playing with the ADC, not good enough for a production unit if better than ''quite light'' vs ''quite dark'' is to be measured. Just visualize the effect the port pin leakage (which is just about the most variable, unstable spec for a chip) will have in this high resistance region. Erik
2012-04-12 01:51 AM
Hi Erik,
Regarding tolerance, I can accept a 10%. Regarding the response time of the LDR, I can accept 50ms and even 100ms In fact I am measuring daylight. After some research on the net, I think it is not a good solution to use an LDR :( That is my own conclusion :(Herzlich,MCU Lüfter
2012-04-12 03:08 AM
Yeah, basically only seen them used here to determine if Sun is up/down, or if it is light/dark, so mainly exterior lighting or panel illumination. Might be viable to measure/log solar exposure on a roof for a solar panel installation.
Erik : I mainly cited the schematic to quickly illustrate the part choice driver, and how the circuit was wired. Pretty sure it's ''science project'' grade rather than targeting more serious application. The part you cited seems a lot more fun/applicable.2012-04-12 07:02 AM
Erik : I mainly cited the schematic to quickly illustrate the part choice driver, and how the circuit was wired.
Clive, no offense, I just wanted to point out that the trap many fall in ''since the manufacturer does it, it MUST be GREAT'' was in place here. Pretty sure it's ''science project'' grade rather than targeting more serious application.
the problem with many posts is that this is rarely stated; however, ''low cost'' made me think it could be a 'real' project. The part you cited seems a lot more fun/applicable.
It is, indeed I have used 10,000s Have fun, Erik
2012-04-12 08:36 AM
beware: TI production status is set to Obsolete..
2012-04-12 09:00 AM
yes, obsolete from TI,they sold the line, I just grabbed the datasheet from the olden days
here is the manufacturer where they are non-obsolete Erik