2012-03-20 8:38 AM
Hi all,
I have recently discovered the STMStudio and I'm trying to make it work with my F4-Discovery. The problem is that when I press play the program CRASH. I have my board attached by USB and ST-link is working good (programming and reading memory with Atollic and STM32 ST-LINK Utility). This is what I do: 1) select ST-LINK SWD, 2) add a variabile for example. ADC3ConvertedValue | 0x2000003c | signed 3)press play -> CRASH! I'm using windows 7 ultimate x64 that's my windows report Firma problema: Nome evento problema: APPCRASH Nome applicazione: STMStudio.exe Versione applicazione: 0.0.0.0 Timestamp applicazione: 45d08242 Nome modulo con errori: StackHash_4937 Versione modulo con errori: 6.1.7601.17725 Timestamp modulo con errori: 4ec49b8f Codice eccezione: c0000374 Offset eccezione: 000ce6c3 Versione SO: 6.1.7601.2.1.0.256.48 ID impostazioni locali: 1040 Informazioni aggiuntive 1: 4937 Ulteriori informazioni 2: 4937eeba3d545f674b9c4a46a5045388 Ulteriori informazioni 3: ed82 Ulteriori informazioni 4: ed824221933476bb1d64a10c354ebfd7 Where am I doing wrong? thanks in advance2012-03-21 8:17 AM
I have tried on another windows 7 x64 machine and it's working good. I can't figure why on my DELL machine isn't working and crashing.
I have disinstalled, repaired the application, installed again java 1.6 and mscrv7.dll but nothing is happening. Keep on crashing! please help thanks2012-04-12 12:57 AM
2012-04-12 6:44 AM
Since I'm using Linux for all boards with workable Linux driver, I have only superficial knowledge about the special requirements for the ST-Link V2 driver.
However, it works on my Acer Laptop with Win 7 64 Bit. I hope you did install the driver and the software as admin, didn't you ? My next step would be to check (USB) driver installation in the device manager, and try a remove + reinstall. Window's driver repair attempts have never been successfull for me. Or, you might have interference with other SW tools...2012-04-12 9:21 AM
Or, you might have interference with other SW tools...
Probably some crap from DELL, seems to be a common factor. Pity no one has a debugger installed, via MSVC or whatever, the dumps don't tend to help much outside Microsoft. Perhaps ST can send someone a build with a .PDB file so you could narrow it down to a source file and line. As everyone has a high-order version of Windows 7, perhaps consider XP Mode via Virtual PC.2012-04-13 7:10 AM
Hi clive1,
I have made a fresh installation on my dell (still win7 x64) without installing demon tools (probably that's the problem) and STMStudio keep working well. I have tried a virtual machine on VirtualBOX from Oracle but I can't easily pass the usb-stlink peripherial. I menage to pass it, only whwn main PC starts and only 1 time. In fact, if I shut down the virtual machine and I try to reboot it, I can't handle the st-link again. It's seems stucked. I think, it's a problem of VirtualBOX and not of stmStudio