2019-02-25 2:23 AM
Hello,
I have a very weird behavior...
When trying to access external synchronous PSRAM.
I see the clock and cs change only if I stop and starts stepping inside the while(1) loop below.
When doing "go", there is no clock nor CS changes.
I tried to add delays as you can see, but nothing helps.
#define FPGA_BANK_ADDR 0x64000000
__IO uint8_t value;
__IO uint8_t * volatile psramaddress = (__IO uint8_t volatile*)FPGA_BANK_ADDR+2;
while(1)
{
*psramaddress = value++;
rd_2 = *psramaddress ;
HAL_Delay(500);
}
Is there any idea ?
Thanks
Solved! Go to Solution.
2019-03-01 12:34 AM
Seems to be like we missed the transaction in scope , and only saw the first transaction for some reason (altough not in trigger mode).
Becuase in software/code, we did have succeeded in continous all registers from fpga, which means that clock transaction, and CS must have toggled for each transaction.
2019-02-25 3:44 AM
Check caching, buffering and sharing setting for memory region and try changing MPU settings.
2019-03-01 12:34 AM
Seems to be like we missed the transaction in scope , and only saw the first transaction for some reason (altough not in trigger mode).
Becuase in software/code, we did have succeeded in continous all registers from fpga, which means that clock transaction, and CS must have toggled for each transaction.