cancel
Showing results for 
Search instead for 
Did you mean: 

BootLoader timeout

yarona
Associate II
Posted on January 12, 2015 at 09:17

Hi

I am using STM32L151 bootloader.

I wanted to run the bootloader at program start, and if no usb if attached for a certain time

go back to regular application.

Is it possible to configure a timeout for the bootloader?

Yaron
1 REPLY 1
Posted on January 12, 2015 at 12:43

The System Loader (BOOT0=High)? or your own Boot Loader?

You can decide whether to call the System Loader from your own code, via a button or RAM setting, but it's not going to timeout and come back to you.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..