2010-11-12 11:21 AM
Bootloader for STM3210E-EVAL?
2011-05-17 5:14 AM
You didn't loose your bootloader, you cannot loose it. Probably your options bytes were accidentally messed up. See this link:
2011-05-17 5:14 AM
Thansk! I loaded the option byte and this what I got.
0x1FFFF800 00FF5AA5 00FF00FF 00FF00FF 00FF00FF Does that look right to you? Do you have a valid option byte for a STM310E-EVAL (STM32F103) that you can send me? I also loaded the flash registers. They are all at their reset value. The ''OPTERR'' bit on ''FLASH_OBR'' had not been set either. Thansk, Ben2011-05-17 5:14 AM
You didn't loose your bootloader, you cannot loose it.
I think Ben is referrering to boot strap code in flash, not the ROM based loader. Pretty much the entire flash rom is game for being bricked. I have a STM3210E-EVAL on the bench, will pull the FLASH image off.(ZIP'd binary attached)2011-05-17 5:14 AM
Thanks clive1! That did the trick! My STM3210E-EVAL is working again. Couple things... I had to power cycle the device. Reset had mirror images of what I was expecting. Also, would you happen to know where in RAM the boot-strap-code is typically located? How can I make that I don't over write it in the future.
Thanks again, Ben