2023-09-18 12:01 PM - edited 2023-09-18 02:59 PM
Hi all, I'm experiencing a strange issue where every once in a while I am unable to enter bootloader on the STM32G0. I have the option bits set correctly and have a hardware push button connected to both nRst and Boot0. I can normally hold the Boot0 button while toggling reset to enter the ST bootloader in ROM. However, every once in a while I enter a state where no matter how many times I reset, or the state of the BOOT0 pin, the device will boot into my application instead of the ROM. The only way to recover seems to be to fully power down the device, after which the bootloader entry continues to work as expected.
It is reproducible on brand new (blank) parts. They enter bootloader by default but after that aren't able enter bootloader by toggling BOOT0 until a power cycle. Outside of that, I haven't been able to deterministically reproduce it, but it does periodically enter this state.
Some notes that may be relevant
Any ideas what this might be or how to debug/resolve?
2023-09-19 07:10 PM
The bootloader and the startup sequence is in ROM and isn't prone to erratic behavior. I would suggest methodically testing, staying objective.
Blank devices will always boot to the bootloader due to an empty flash check--no surprise there.
Having ST-Link connected during boot is going to control the BOOT0 pin, so you'll need to go the option byte route if you want to choose what should load.
2023-09-26 02:18 PM - edited 2023-09-26 02:23 PM
Okay, I did some more digging and this is reproducible on a NUCLEO-G071RB. See steps below
Configure option bytes using STM32 Cube Programmer:
Reproduce expected behavior:
Reproducing breaking behavior. Starting from step 5 above:
At this point you can reset the board as much as you want, it will not go back to the ROM. If I disconnect the external 5V and reconnect it, everything starts working again. Is this expected behavior? This debugger cycling obviously isn't a common use case, but I have observed these same symptoms without connecting an ST-Link at all, leaving the G0 in an unrecoverable state until a full power cycle.
2023-09-27 07:53 PM
2023-09-29 02:39 PM
I'm not trying to change the bytes though. I set them once and then keep them the same. All I'm doing is powering up and the powering down the ST-Link on board the Nucleo. Is there anything else that latches?