2018-05-29 9:41 PM
what happen if I don't push the boot0 pin on Vdd or pull it to Vss, just let it float ?
2018-05-29 10:52 PM
Hello,
In such a case state of BOOT0 pin will depend on the external conditions. It can 'catch' some disturbances and be either 'H' or 'L' state. Thus it may happened that MCU will not start from internal FLASH (Boot0='L') but it will try to run from system memory (built in bootloader) or internal SRAM. Thus I would strongly recommend to fix the level on this pin during startup process of the MCU.
Best regards,
Artur
2018-05-29 10:55 PM
run a 1k - 10K to ground for normal operation.
2018-05-30 2:10 AM
,
,
Thank you so much !
2018-05-30 12:56 GMT+07:00 T J <,st-microelectronics@jiveon.com>,:
STMicroelectronics Community
<,https://community.st.com/?et=watches.email.thread>,
Re: Boot0 Pin
reply from T J
<,
MCUs Forum* - View the full discussion
<,https://community.st.com/0D70X000006Ss7wSAC
2018-05-30 3:00 AM
Huy Nguyen wrote:
Thank you so much !