cancel
Showing results for 
Search instead for 
Did you mean: 

Bit levels matter

Pavel A.
Evangelist III

Anyone seen this? The politically-correctness crap gets to EE...

https://www.oshwa.org/a-resolution-to-redefine-spi-signal-names/

5 REPLIES 5

I'm not sure how this addresses current day slavery, which is still prevalent.

Or issues with conflict minerals. They aren't fixed with paperwork, or related time wasting exercises.

Shouldn't we be remediating these issues at the source?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Just to increase wokeness on new confusing four-letter-isms we may come across.

So, "SDIO" these days can read "serial data in-out", PICO - "peripheral in/controller out", etc.

But wait, there are timers. What could they call master/slave timers? :face_without_mouth:

S.Ma
Principal

What is important is intuitive name that makes us move forward faster in a project. MOSI and MISO are IMHO more intuitive to connect that Uart RX and TX which caused modem and non null modem cable mess and scraps. So until there is a completely better proposal... maybe like usb host and device HODI and HIDO ?....

gbm
Lead III

How about BOwI and BIwO? Should count as politically correct...

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice

That's pretty simple: "Proud Color Timer" and "ashamed to be white timer".

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice