cancel
Showing results for 
Search instead for 
Did you mean: 

Bad linker file with CubeMx

CAPOSIENA.Philippe
Associate II
Posted on July 20, 2015 at 17:49

Hello,

i'm using a STM32F334C8 with STM32CubeMx and with Atollic True Studio or SW4STM32.

When i generate a project with STM32CubeMx (for TrueStudio or SW4STM32) the linker file is wrong. I get a 16ko size ram instead of 12ko. When i try to debug, an address error occurs. I have to manually modify the linker file (*.ld) and after everything is ok.

When i create a project with True Studio only, the linker file is ok.

This is very strange. Is it a bug or do i miss something ?

Thanks
4 REPLIES 4
stm32cube-t
Senior III
Posted on August 27, 2015 at 19:41

Dear user,

These are known issues. Please upgrade to next Cube MX 4.10 when it is released next week.

Best regards
CAPOSIENA.Philippe
Associate II
Posted on August 31, 2015 at 10:16

Hello,

i updated CubeMx to 4.10 but this bug has not been fixed.

Philippe

stm32cube-t
Senior III
Posted on September 01, 2015 at 16:08

Dear user,

You are correct. The issue has been logged.

Thank you for your feedback.
stm32cube-t
Senior III
Posted on February 09, 2016 at 12:05

Dear user,

The issue is now fixed in STM32CubeMX 4.13.