cancel
Showing results for 
Search instead for 
Did you mean: 

B-L462E-CELL1 eSIM activation is not allowed in this PLMN

Nelson_Huang
Associate

Hello, 

After purchasing the pre-configured Truphone eSIM B-L462E-CELL1 kit and following the eSIM activation steps, I still haven't seen the eSIM marked as activated on the Truphone IoT dashboard after one day.

I've also seen others inquire about this issue and have followed the advice to set 'at%nwoper' to "TRUPHONE" in the response, but the eSIM still cannot be activated.
(reference: https://community.st.com/t5/stm32-mcus-embedded-software/b-l462e-cell1-esim-activation-failed/m-p/617775)

 

Log:

AUTOM TASK: WAITING_FOR_NETWORK_STATUS_STATE - POLLING_TIMER_EVENT
*********** CST_network_status_test_mngt ********
ATParser:*** SEND (size=10) ***
AT+CEREG?<CR>
<CR><LF>
+CEREG: 2,3<CR><LF>
ATCModem:NetworkState (EPS) = REGISTRATION_DENIED
<CR><LF>
OK<CR><LF>
ATParser:*** SEND (size=9) ***
AT+CREG?<CR>
<CR><LF>
+CREG: 2,0<CR><LF>
ATCModem:NetworkState (CS) = NOT_REGISTERED_NOT_SEARCHING
<CR><LF>
OK<CR><LF>
ATParser:*** SEND (size=9) ***
AT%CEER?<CR>
<CR><LF>
%CEER: 1,"NAS-EMM","ATTACH","REJECT",#14,EPS_SERVICES_NOT_ALLOWED_IN_THIS_PLMN<CR><LF>
<CR><LF>
OK<CR><LF>
ATParser:*** SEND (size=9) ***
AT+COPS?<CR>
<CR><LF>
+COPS: 0<CR><LF>
<CR><LF>
OK<CR><LF>
ATParser:*** SEND (size=7) ***
AT+CSQ<CR>
<CR><LF>
+CSQ: 99,99<CR><LF>
<CR><LF>
OK<CR><LF>
-Sig quality rssi : 99
-Sig quality ber : 99
<CR><LF>
%NOTIFYEV:"SIMREFRESH",2,6,"00000000000000"<CR><LF>

Could you help to resolve this problem?
The attached file is full of logs.

 

Thanks a lot

Nelson

4 REPLIES 4
STTwo-32
ST Employee

Hello @Nelson_Huang and welcome to the ST Community :smiling_face_with_smiling_eyes:.

I suggest you to take a look at the this post.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello,

I've dragged and dropped this binary file onto my device using ST LINK, please help to check.

 

Log:

===== X-Cube-Cellular version : X-CUBE-CELLULAR-7.1.0 =====

TYPE1SC UART config: BaudRate=115200 / HW flow ctrl=1
Get IP Address...
SysCtrl_TYPE1SC:MODEM POWER ON
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCore:TIMEOUT EVENT(1000 ms)
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCModem:Tempo started (3000 ms)...
ATCore:TIMEOUT EVENT(3000 ms)
Modem Boot OK, sim slot nb 0
LOG ERROR #1: channel=1 / errorId=7 / gravity=2
LOG ERROR #2: channel=2 / errorId=1 / gravity=2
STM32 IP Address: 0.0.0.0
DNS Server address: 8.8.8.8
SNTP Time Sync... 0.pool.ntp.org
SysCtrl_TYPE1SC:modem channel closed
SysCtrl_TYPE1SC:MODEM POWER OFF
SysCtrl_TYPE1SC:MODEM POWER ON
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCore:TIMEOUT EVENT(1000 ms)
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCModem:Tempo started (3000 ms)...
ATCore:TIMEOUT EVENT(3000 ms)
Modem Boot OK, sim slot nb 0
LOG ERROR #3: channel=1 / errorId=7 / gravity=2
LOG ERROR #4: channel=2 / errorId=1 / gravity=2
SysCtrl_TYPE1SC:modem channel closed
SysCtrl_TYPE1SC:MODEM POWER OFF
SysCtrl_TYPE1SC:MODEM POWER ON
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCore:TIMEOUT EVENT(1000 ms)
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCModem:Tempo started (3000 ms)...
ATCore:TIMEOUT EVENT(3000 ms)
Modem Boot OK, sim slot nb 1
LOG ERROR #5: channel=1 / errorId=7 / gravity=2
LOG ERROR #6: channel=2 / errorId=1 / gravity=2
SysCtrl_TYPE1SC:modem channel closed
SysCtrl_TYPE1SC:MODEM POWER OFF
SysCtrl_TYPE1SC:MODEM POWER ON
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCore:TIMEOUT EVENT(1000 ms)
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCModem:Tempo started (3000 ms)...
ATCore:TIMEOUT EVENT(3000 ms)
Modem Boot OK, sim slot nb 1
ATCModem:Tempo started (2000 ms)...
ATCore:TIMEOUT EVENT(2000 ms)
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCore ERROR:AT_sendcmd error
ATCore ERROR:AT_sendcmd error: parse from rsp
LOG ERROR #7: channel=1 / errorId=11 / gravity=2
LOG ERROR #8: channel=1 / errorId=14 / gravity=2
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (CS) = NOT_REGISTERED_NOT_SEARCHING
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (CS) = NOT_REGISTERED_NOT_SEARCHING
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (CS) = NOT_REGISTERED_NOT_SEARCHING
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (CS) = NOT_REGISTERED_NOT_SEARCHING
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (CS) = NOT_REGISTERED_NOT_SEARCHING
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (CS) = NOT_REGISTERED_NOT_SEARCHING
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (CS) = NOT_REGISTERED_NOT_SEARCHING
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (CS) = NOT_REGISTERED_NOT_SEARCHING
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (CS) = NOT_REGISTERED_NOT_SEARCHING
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (CS) = NOT_REGISTERED_NOT_SEARCHING
ATCModem:NetworkState (EPS) = REGISTRATION_DENIED
ATCModem:NetworkState (CS) = NOT_REGISTERED_NOT_SEARCHING
ATCModem:NetworkState (EPS) = REGISTRATION_DENIED
ATCModem:NetworkState (CS) = NOT_REGISTERED_NOT_SEARCHING
ATCModem:NetworkState (EPS) = REGISTRATION_DENIED
ATCModem:NetworkState (CS) = NOT_REGISTERED_NOT_SEARCHING

 

The attached file is full of logs.

Thanks, 

Nelson

Semyalo
Associate II

Hello,

I'm almost facing a similar error;
"ATCModem:NetworkState (EPS) = NOT_REGISTERED_NOT_SEARCHING"
"AT%CEER?<CR> %CEER: 1,"NAS-EMM","ATTACH","REJECT",#11,PLMN_NOT_ALLOWED<CR><LF>"

- The eSIM is already activated on the Truphone IoT dashboard
- Running "at at%nwoper?" command gives "TRUPHONE".
- South Korea is covered for LTE-M by Truephone (https://www.truphone.com/things/plans/coverage/?feature=LTE-M&addon=Asia )

Check the attached TeraTerm serial log for more details.
How can I resolve this error?

Thanks for your help.
Kind regards.

 

I got a solution, it seems the modem FW wasn’t configured to LTE CATM, so I configured it with reference to @S.RA  and @McLovin at;

https://community.st.com/t5/stm32-mcus-embedded-software/i-need-help-with-an-issue-regarding-stm32l462re-bl462ecell1-how/m-p/211110#M13406.
https://community.st.com/t5/stm32-mcus-embedded-software/i-need-help-with-an-issue-regarding-stm32l462re-bl462ecell1-how/m-p/211114#M13410
I used the commands; “at at%getacfg=radiom.config.preferred_rat_list” and

“at at%setacfg=radiom.config.preferred_rat_list,"CATM"”.
Afterward, the connection was established within 50 seconds.
Regards.