cancel
Showing results for 
Search instead for 
Did you mean: 

available SPIs on STM3210E-EVAL

supercoolman
Associate II
Posted on February 22, 2010 at 04:52

available SPIs on STM3210E-EVAL

2 REPLIES 2
steven239955
Associate
Posted on May 17, 2011 at 13:41

SPI1 is connected to the serial flash, Its the M25P64 chip on the board, not a removeable media. You can use the SPI1 for whatever you want once you re-map it to its alternate function pins - don't think there is a conflict then.

chikos332
Associate II
Posted on May 17, 2011 at 13:41

Hi,

If you have the Serial Wire Jtag feature (SWJ) on your programmer you can use the SPI3 at the same time with debugging. You just have to configure the STM32 to work in SWJ mode.