2009-05-04 11:03 PM
Application runs in RLINK debugger but not properly without it
2011-05-17 04:11 AM
Dear poor suffering software developer ;-)
the problem described under subject appears in a bootloader (iap) application. The bootloader should start and send a start message to a terminal programm. The message never appears, but the software was running. It seems that only the start message disappears. The solution: I added a delay (200ms) because the STM32 starts very early from reset. The voltage is not raised to the full level. So the RS-232 driver haven't enough voltage and the message doesn't go out. Maybe it helps someone of you... Best regards pt1 [ This message was edited by: pt1 on 05-05-2009 16:57 ]