cancel
Showing results for 
Search instead for 
Did you mean: 

Application runs in RLINK debugger but not properly without it

pt1
Associate II
Posted on May 05, 2009 at 08:03

Application runs in RLINK debugger but not properly without it

1 REPLY 1
pt1
Associate II
Posted on May 17, 2011 at 13:11

Dear poor suffering software developer ;)

the problem described under subject appears in a bootloader (iap) application.

The bootloader should start and send a start message to a terminal programm. The message never appears, but the software was running. It seems that only the start message disappears. The solution: I added a delay (200ms) because the STM32 starts very early from reset. The voltage is not raised to the full level. So the RS-232 driver haven't enough voltage and the message doesn't go out.

Maybe it helps someone of you...

Best regards pt1

[ This message was edited by: pt1 on 05-05-2009 16:57 ]