cancel
Showing results for 
Search instead for 
Did you mean: 

[AN2834] Is the LM235 a temperature sensor or voltage reference? (Errata?)

Not applicable

​Hi,

Maybe the TL431 is a voltage reference.

This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7

LM236 ? But I think that's a hack of the LM235 with a leg cropped off...

https://www.ti.com/lit/ds/symlink/lm336-2.5.pdf?ts=1655053986350&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FLM336-2.5

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

(Does the website only accept 1 attachment in responses?)

I don't believe it was done on purpose, I believe it might be a typo, and the text editor went on to suggest the LM235. The equivalent internal schematic is not the same for LM235 and LM236.

 

>>I don't believe it was done on purpose..

Have to be super-class dyslexic to get from LM235 to TL431

Much more probable it's being used as a QND two-terminal shunt voltage reference, NatSemi style, and in the context of the quoted usage.

@Peter BENSCH​ do you have an examples of this usage within ST?

You can only have a single file attachment per post, but can add multiple images.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Not applicable

Let me understand:

1- LM235 is what is in the referred document AN2834.

2- TL431 I cited as an example of what a voltage reference is.

3- LM236 was quoted later (which seems to be better suited to be in the document rather than LM235)

4- Dyslexia is quite real these days, and is more evident when a person is tired.

5- This question is directed to ST employees who have access to review the document.

6- I don't mean to be rude, but apart from the LM236 quote there seems to be no addition when commenting on other things.

7- Thank you for your attention.

Peter BENSCH
ST Employee

@Community member​ Thanks for bringing this to our attention. Indeed, the LM235 is a temperature sensor and the reference in AN2834 is therefore a typo. As a voltage reference for 2.5V, you can use instead e.g. TL1431A (0.25%) or TS824AILT-2.5 (0.5%), which are also available with lower accuracy (without suffix A).

I don't have an application example at the moment, but the use of Vref+ should be quite easy as long as you respect the permissible voltage range for Vref+ and decouple GND and Vref+ cleanly (appropriate layout, LC filter, possibly ferrites).

Regards

/Peter

@Amel NASRI​ Please pass this on to the division so that the typing error can be corrected.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi All,

We confirm that this is a typo where LM236 is meant as already mentioned in page 25 of the same document.

The application note will be updated to replace LM23x by TL1431A as a reference voltage.

Internal ticket number: 130288 (This is an internal tracking number and is not accessible or usable by customers).

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.