2024-03-06 1:44 PM
Hi, I'm trying to write an algorithm to load into external memory in QSPI_Dual_mode MT25QL512A for KEIL. I followed this instruction. The algorithm works BUT! when the firmware exceeds 90040001H an error occurs during verification. Smaller programs are flashed and work fine.
Programming External Flash with STM32 Devices
2024-03-06 1:56 PM
So failing 256 KB in
Either issue with Erasure, or content written incorrectly, or into the wrong location.
You can instrument the algorithm to output diagnostic info via a serial port
2024-03-06 2:00 PM
If you set “erase full chip” then the error disappears, apparently the problem is in erasing the sector, as I understand it, the algorithm erases only the first 2 sectors.
2024-03-06 2:01 PM
this is a good idea, otherwise I couldn’t understand how to debug this code =))
2024-03-06 2:43 PM
Not seeing anything egregious in there, perhaps a couple of things I'd approach differently.
BSP_QSPI_GetStatus() only checks one IC. Needs to read 2 bytes and check both
The erase block size will be 128KB, page write size is 512B for DUAL
Not immediately failing, so not an errant load (Winbond / Macronix) setting Block Protection bits.
MT25TL01G / DUAL MT25QL512A
PB2:AF9 CLK
PG6:AF10 NCS
PD11:AF9 BK1_IO0
PF9:AF10 BK1_IO1
PF7:AF9 BK1_IO2
PF6:AF9 BK1_IO3
PH2:AF9 BK2_IO0
PH3:AF9 BK2_IO1
PG9:AF9 BK2_IO2
PG14:AF9 BK2_IO3
Not spent a lot of time on these as ST provides programmer for these parts as they use them. Will check the build system when I get home as I have other FLM / STLDR projects.
2024-03-06 7:10 PM - edited 2024-03-06 7:33 PM
https://github.com/cturvey/stm32extldr/blob/main/h7_mt25tl01g/README.md
CUSTOM24 PB2, PG6, PD11, PF9, PF7, PF6, PH2, PH3, PG9, PG14 (KEIL/FLM)
https://github.com/cturvey/stm32extldr/blob/main/h7_mt25ql512a/MT25QL512A_STM32H7XX-CUSTOM24.FLM