2024-03-14 4:19 AM - edited 2024-03-14 4:49 AM
Hi,
I tried to reach 1us delay. To do that I use a timer on 1MHz and try to reach more or less precision delay.
void delayMicro(uint16_t delayMc) {
__HAL_TIM_SET_COUNTER(&htim16,0); // set the counter value a 0
while (__HAL_TIM_GET_COUNTER(&htim16) < delayMc);
}
HAL_TIM_Base_Start(&htim16);
while () {
delayMicro(100);
HAL_GPIO_TogglePin(OUT1_GPIO_Port, OUT1_Pin);
}
And the result is always desired delay+6-8us
Even if I set delay = 1us, I get 7-8us.
I did something wrong or is this GPIO or microcontroller limitation?
Solved! Go to Solution.
2024-03-14 6:41 AM
> And the result is always desired delay+6-8us
Overhead. Your timer has a precision of 1us, so expect some jitter due to that.
7us on a 12 MHz chip is 84 ticks. That's not a lot. You're jumping/returning to a function, dereferencing pointers, accessing registers. Likely compiling under Release mode would do much better. Using direct register access will help a bit.
2024-03-14 4:33 AM
You don't show any of the TIM initialization code.. check prescaler, check clocking via MCO pin.
You don't want to have interrupts.
Perhaps easier to delta the TIM16->CNT than keep resetting
2024-03-14 4:46 AM
>I did something wrong or is this GPIO or microcontroller limitation?
You did more than something wrong.
2024-03-14 4:46 AM
htim16.Instance = TIM16;
htim16.Init.Prescaler = 11;
htim16.Init.CounterMode = TIM_COUNTERMODE_UP;
htim16.Init.Period = 65534;
htim16.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim16.Init.RepetitionCounter = 0;
htim16.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
And I don't use interrupt for this timer.
Implementing delta for CNT didn't help.
2024-03-14 6:41 AM
> And the result is always desired delay+6-8us
Overhead. Your timer has a precision of 1us, so expect some jitter due to that.
7us on a 12 MHz chip is 84 ticks. That's not a lot. You're jumping/returning to a function, dereferencing pointers, accessing registers. Likely compiling under Release mode would do much better. Using direct register access will help a bit.
2024-03-14 7:18 AM
Yeah, I think the same but hope that I'm wrong. :)
2024-03-14 8:13 AM
Strange but even on 48MHz and release build I got 102uS instead 100us.
2024-03-14 8:44 AM
96 ticks of overhead is consistent with what you saw at 12 MHz clock.
I would guess about half of the overhead is within HAL_GPIO_TogglePin itself.
2024-03-15 6:35 PM
My belated thoughts -
Agree with Tesla, don't bother resetting the counter, just use it as a reference and compare it with a register/variable with a delta added to it.
If these things are critical, I would be doing something in assembler to minimise overheads (including loop overheads).