after configuring standby Jlink connection is lost
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-08-10 1:29 PM
I am working with STM32L051 and need to enter STANDBY mode.
The configuration and entering STANDBY are as follows:/******************************************************/
static void SystemPower_Config(void)
{
/* Enable Power Control clock */
__HAL_RCC_PWR_CLK_ENABLE();
/* Enable Ultra low power mode */
HAL_PWREx_EnableUltraLowPower();
/* Enable the fast wake up from Ultra low power mode */
HAL_PWREx_EnableFastWakeUp();
/* Enable debug in standby *.
DBGMCU->CR |= 0x00000004;
}
/******************************************************/
static void Enter_standby(void)
{
/* The Following Wakeup sequence is highly recommended prior to each Standby mode entry
mainly when using more than one wakeup source this is to not miss any wakeup event.
- Disable all used wakeup sources,
- Clear all related wakeup flags,
- Re-enable all used wakeup sources,
- Enter the Standby mode.
*/
/* Disable all used wakeup sources: PWR_WAKEUP_PIN1 */
HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN1);
/* Clear all related wakeup flags*/
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
/* Enable WakeUp Pin PWR_WAKEUP_PIN1 */
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
/* Enter the Standby mode */
HAL_PWR_EnterSTANDBYMode();
}
After programming I can't access a controller by JLink, even for programming,
though controller IS NOT in standby mode. Messages are: - No Cortex-M SW Device Found - Error: Flash Download failed - Target DLL has been cancelled. Power cycling doesn't help. Is there any way to restore connectivityor completely reset the microcontroller ?- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-08-10 1:40 PM
Pull BOOT0 High, Reset, Connect, Erase
You could also change ''Connect Under Reset'' optionsUp vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-08-10 2:15 PM
It worked, thanks a lot!
Also I couldn't find 'Connect Under Reset' option.Could you please tell me where is it?Thank you again,Gennady- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-08-10 3:11 PM
Too early to celebrate :(
I erased a chip, restored BOOT0 at GND.Now I can program a chip, but it doesn't start.On debugging I can see that it resets to 0x1FF00238.Once in a while it resets to normal 0x80000D4, and then it works on debug.But it never starts on a board, on a power cycle.Have I done something wrong?- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-08-10 3:56 PM
Pulling BOOT0 to ground should suffice.
The connection options for the debugger are in the lower left of the Keil Debugger Settings window.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-08-10 6:41 PM
BOOT0 is at the GND.
Still resets to 0x1FF00238 and doesn't run on a board.