cancel
Showing results for 
Search instead for 
Did you mean: 

Address calculation using sizeof() operator

KAJIK.1
Associate III

I am a little bit confusing with Address calculation using sizeof() operator.

I am writing a program for DMA transfer half a buffer in a time.

Such as,

---------

   1st:      HAL_SPI_Transmit_DMA(&hspi1, ptr1, buf_len/2) ;

   2nd:     HAL_SPI_Transmit_DMA(&hspi1, ptr2, buf_len/2) ;

---------

  where ptr1 is pointer to DATA[0] and ptr2 is pointer to DATA[10].

However, when I wrote 2nd one as,

---------

     HAL_SPI_Transmit_DMA(&hspi1, ptr1+sizeof(uint16_t)*10, buf_len/2) ;

---------

I got wrong addres for ptr2.

Therefore, I checked the result of sizeof() as below, and found sizeof(uint16_t) does not return same value in address calculation.

---------

  uint16_t Data[20] ;

  uint16_t * addr0 = Data ;          // 0x2000ffbc or 536936380   [base]

  uint16_t * addr1 = &(Data[10]) ;   // 0x2000ffe4 or 536936420   [base + 20]

  uint16_t * addr2 = Data + sizeof(uint16_t)*10 ; // 0x2000ffd0 or 536936400 [base + 40]

  int size = sizeof(uint16_t) ; // size = 2

  int arraysize = sizeof(Data) / sizeof(Data[0]) ; // arraysize = 20

---------

​I suppose uint16_t is 2 byte data as shown in sizeof(uint16_t).  Otherwise how can I align 2 byte data in a buffer?

Kindly enlighten me!

Thank you,

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
TDK
Super User

Incrementing a pointer of type (uint16_t *) increases its address by the size of the value it points to, which is 2 in this case.

So instead of doing "Data + sizeof(uint16_t)*10", you should just be doing "Data + 10".

int arraysize = sizeof(Data) / sizeof(Data[0])  = 40 / 2 = 20;

Seems fine to me. sizeof(Data) is the size in bytes of the Data array.

If you feel a post has answered your question, please click "Accept as Solution".
KAJIK.1
Associate III

Dear TDK,

Thank you very much for your kind answer.

I understood as this.

Address calculation is not done in byte, but done in sizeof(Data) or sizeof(Data_type).

Therefore, I should have written 2nd case as, (not checked yet.)

HAL_SPI_Transmit_DMA(&hspi1, (uint16_t *)((uint8_t*)ptr1+sizeof(uint16_t)*10), buf_len/2) ;

Many thanks.

Pavel A.
Super User

This is why the Go language dumped pointer arithmetic. Too confusing for modern coders.

-- pa

Piranha
Chief II

> Address calculation is not done in byte, but done in sizeof(Data) or sizeof(Data_type).

The first is wrong, the second is right. In fact is even simpler - the ptr1 pointer address calculation is done in units of sizeof(*ptr1).

> Therefore, I should have written 2nd case as... (uint8_t*)ptr1+sizeof(uint16_t)*10

It's correct, but terrible. TDK already told you what to write! It's just ptr1 + 10 or &ptr1[10].

> Too confusing for modern coders.

The above example... If a "developer" is not able of grasping such a trivial thing, he's not able of developing anything useful anyway.