cancel
Showing results for 
Search instead for 
Did you mean: 

ADC VEREFINT Calibration value and VREFINT_DATA of STM32L100RBT6

sanctified
Associate II

Hi,

I want to use the VEREFINT to get the voltage of my battery.

According to the formula provided by the datasheet (screenshot attached), I need the VREFINT calibration value and the VREFINT_DATA.

What is the register to read the calibration value from? I didn't find this in the datasheet.

The same for the VREFINT_DATA. For the VREFINT_DATA I think it's stored in the specific data address VREFINT_Factory_CONV byte but I do not find in the datasheet what this address is.

0693W000006FgIpQAK.jpg 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Please don't be confused by datasheets and reference manuals, you are currently referring to the RM0038, section 12.12 (pg. 287 in rev 16).

According the datasheet of the STM32L100RBT6-A, section 6.3.3, VREFINT_CAL can be obtained from 0x1FF80078...0x1FF80079.

A supply-relative ADC measurement always requires two measurements:

  • the signal to be measured relative to the supply voltage and
  • a reference voltage, e.g. the internal, also relative to the supply voltage

RM0038 says that VREFINT_DATA is the actual VREFINT output value converted by the ADC. In this case this is the second measurement mentioned above.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Please don't be confused by datasheets and reference manuals, you are currently referring to the RM0038, section 12.12 (pg. 287 in rev 16).

According the datasheet of the STM32L100RBT6-A, section 6.3.3, VREFINT_CAL can be obtained from 0x1FF80078...0x1FF80079.

A supply-relative ADC measurement always requires two measurements:

  • the signal to be measured relative to the supply voltage and
  • a reference voltage, e.g. the internal, also relative to the supply voltage

RM0038 says that VREFINT_DATA is the actual VREFINT output value converted by the ADC. In this case this is the second measurement mentioned above.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.