cancel
Showing results for 
Search instead for 
Did you mean: 

ADC multichannel DMA

meena
Associate III

with all your help I tried to change multichannel using DMA but I cant able to read the values can anyone please help

 

ADC_HandleTypeDef hadc1; DMA_HandleTypeDef hdma_adc1; UART_HandleTypeDef huart2; /* USER CODE BEGIN PV */ uint16_t mains=0; uint16_t battV=0; uint16_t tsense=0; uint16_t battI=0; uint16_t ledI=0; uint16_t opv=0; uint16_t batMon=0; uint32_t getADCvalues[7]; char msg[100]; *********** /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_DMA_Init(void); static void MX_ADC1_Init(void); static void MX_USART2_UART_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ uint8_t convCompleted=0; void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc) { convCompleted=1; } /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_DMA_Init(); MX_ADC1_Init(); MX_USART2_UART_Init(); /* USER CODE BEGIN 2 */ HAL_ADC_Start_DMA(&hadc1, (uint32_t *)getADCvalues, 7); /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ while(!convCompleted); for(uint8_t i =0;i< hadc1.Init.NbrOfConversion;i++) { tsense=getADCvalues[0]; ledI=getADCvalues[1]; battI=getADCvalues[2]; mains=getADCvalues[3]; opv=getADCvalues[4]; batMon=getADCvalues[5]; battV=getADCvalues[6]; } static void MX_USART2_UART_Init(void) { /* USER CODE BEGIN USART2_Init 0 */ /* USER CODE END USART2_Init 0 */ /* USER CODE BEGIN USART2_Init 1 */ /* USER CODE END USART2_Init 1 */ huart2.Instance = USART2; huart2.Init.BaudRate = 115200; huart2.Init.WordLength = UART_WORDLENGTH_8B; huart2.Init.StopBits = UART_STOPBITS_1; huart2.Init.Parity = UART_PARITY_NONE; huart2.Init.Mode = UART_MODE_TX_RX; huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart2.Init.OverSampling = UART_OVERSAMPLING_16; huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; huart2.Init.ClockPrescaler = UART_PRESCALER_DIV1; huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; if (HAL_UART_Init(&huart2) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USART2_Init 2 */ /* USER CODE END USART2_Init 2 */ } /** * Enable DMA controller clock */ static void MX_DMA_Init(void) { /* DMA controller clock enable */ __HAL_RCC_DMA1_CLK_ENABLE(); /* DMA interrupt init */ /* DMA1_Channel1_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn); }
View more

 

how to read these values in debugger with Live expression I couldn't get that 

9 REPLIES 9
TDK
Guru

> I cant able to read the values

Why cant you able to read the values? What happens when you try?

ADC values should probably be uint16_t, not uint32_t. They should also be marked volatile, as they're modified outside of the program.

If you feel a post has answered your question, please click "Accept as Solution".
meena
Associate III

the values are still 0 for all 

 

liaifat85
Senior III

make sure that your DMA configuration, especially the memory address where ADC values are being stored, is correct. The getADCvalues array should be the correct destination for DMA to store the ADC values.

Debug your program. Hit pause, see where execution is at and examine the state of the variables in a non-live expression context.

If you feel a post has answered your question, please click "Accept as Solution".
meena
Associate III

Is any otherways to read adc values for sequencer not fully configured mode as using channel 16 and channel 15.

I have tried it witout DMA but seems to getting all values same I am stuck at a project to proceed as we need adc values to proceed

Your posts are all over the place, hard to know what you need help with. Nothing about channels 15/16 in original post, or any mention of ADC configuration at all for that matter.

Can't debug what I can't see.

If you feel a post has answered your question, please click "Accept as Solution".
meena
Associate III

Thanks for your kind response and help here i have attached the entire code and what values i am getting debugger .If you can please check.this I have done by polling

unsigned short Temp,Vbat,BattI,Opv,LedI,Batt_Mon; /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_ADC1_Init(void); static void MX_TIM3_Init(void); static void MX_TIM1_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ void ADC_Vbat(void) { ADC_ChannelConfTypeDef sConfig = {0}; sConfig.Channel = ADC_CHANNEL_16; sConfig.Rank = ADC_RANK_CHANNEL_NUMBER; sConfig.SamplingTime = ADC_SAMPLINGTIME_COMMON_1; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } HAL_ADC_Start(&hadc1); HAL_ADC_PollForConversion(&hadc1, 1000); Vbat = HAL_ADC_GetValue(&hadc1); HAL_ADC_Stop(&hadc1); } void ADC_BattIsense(void) { ADC_ChannelConfTypeDef sConfig = {0}; sConfig.Channel = ADC_CHANNEL_3; sConfig.Rank = ADC_RANK_CHANNEL_NUMBER; sConfig.SamplingTime = ADC_SAMPLINGTIME_COMMON_1; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } HAL_ADC_Start(&hadc1); HAL_ADC_PollForConversion(&hadc1, 1000); BattI = HAL_ADC_GetValue(&hadc1); HAL_ADC_Stop(&hadc1); } void ADC_ledIsense(void) { ADC_ChannelConfTypeDef sConfig = {0}; sConfig.Channel = ADC_CHANNEL_2; sConfig.Rank = ADC_RANK_CHANNEL_NUMBER; sConfig.SamplingTime = ADC_SAMPLINGTIME_COMMON_1; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } HAL_ADC_Start(&hadc1); HAL_ADC_PollForConversion(&hadc1, 1000); LedI = HAL_ADC_GetValue(&hadc1); HAL_ADC_Stop(&hadc1); } void ADC_Temp(void) { ADC_ChannelConfTypeDef sConfig = {0}; sConfig.Channel = ADC_CHANNEL_0; sConfig.Rank = ADC_RANK_CHANNEL_NUMBER; sConfig.SamplingTime = ADC_SAMPLINGTIME_COMMON_1; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } HAL_ADC_Start(&hadc1); HAL_ADC_PollForConversion(&hadc1, 1000); Temp = HAL_ADC_GetValue(&hadc1); HAL_ADC_Stop(&hadc1); } void Open_Circuit(void) { ADC_ChannelConfTypeDef sConfig = {0}; sConfig.Channel = ADC_CHANNEL_9; sConfig.Rank = ADC_RANK_CHANNEL_NUMBER; sConfig.SamplingTime = ADC_SAMPLINGTIME_COMMON_2; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } HAL_ADC_Start(&hadc1); HAL_ADC_PollForConversion(&hadc1, 1000); Opv = HAL_ADC_GetValue(&hadc1); HAL_ADC_Stop(&hadc1); } void Batt_Monitor(void) { ADC_ChannelConfTypeDef sConfig = {0}; sConfig.Channel = ADC_CHANNEL_15; sConfig.Rank = ADC_RANK_CHANNEL_NUMBER; sConfig.SamplingTime = ADC_SAMPLINGTIME_COMMON_2; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } HAL_ADC_Start(&hadc1); HAL_ADC_PollForConversion(&hadc1, 1000); Batt_Mon = HAL_ADC_GetValue(&hadc1); HAL_ADC_Stop(&hadc1); } /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_ADC1_Init(); MX_TIM3_Init(); MX_TIM1_Init(); /* USER CODE BEGIN 2 */ /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { ADC_Vbat(); ADC_BattIsense(); ADC_ledIsense(); ADC_Temp(); Open_Circuit(); Batt_Monitor(); /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ /* USER CODE END 3 */ } } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Configure the main internal regulator output voltage */ HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1); /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1; RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV1; RCC_OscInitStruct.PLL.PLLN = 6; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV4; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK) { Error_Handler(); } } /** * @brief ADC1 Initialization Function * @PAram None * @retval None */ static void MX_ADC1_Init(void) { /* USER CODE BEGIN ADC1_Init 0 */ /* USER CODE END ADC1_Init 0 */ ADC_ChannelConfTypeDef sConfig = {0}; /* USER CODE BEGIN ADC1_Init 1 */ /* USER CODE END ADC1_Init 1 */ /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion) */ hadc1.Instance = ADC1; hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2; hadc1.Init.Resolution = ADC_RESOLUTION_12B; hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc1.Init.ScanConvMode = ADC_SCAN_SEQ_FIXED; hadc1.Init.EOCSelection = ADC_EOC_SEQ_CONV; hadc1.Init.LowPowerAutoWait = DISABLE; hadc1.Init.LowPowerAutoPowerOff = DISABLE; hadc1.Init.ContinuousConvMode = DISABLE; hadc1.Init.NbrOfConversion = 6; hadc1.Init.DiscontinuousConvMode = DISABLE; hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START; hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; hadc1.Init.DMAContinuousRequests = DISABLE; hadc1.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN; hadc1.Init.SamplingTimeCommon1 = ADC_SAMPLETIME_19CYCLES_5; hadc1.Init.OversamplingMode = DISABLE; hadc1.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH; if (HAL_ADC_Init(&hadc1) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_0; sConfig.Rank = ADC_RANK_CHANNEL_NUMBER; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_2; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_3; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_9; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_15; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_16; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN ADC1_Init 2 */ /* USER CODE END ADC1_Init 2 */ }
View more

meena_0-1700654363488.png

 

TDK
Guru

Your MX_ADC1_Init is set up to initialize the ADC for 6 conversions, but then you're trying to do single conversions. Might be other issues as well.

Perhaps go off of a working example code from the MX repository.

Here's an example for multiple conversions using DMA:

https://github.com/STMicroelectronics/STM32CubeG0/tree/master/Projects/NUCLEO-G070RB/Examples/ADC/ADC_MultiChannelSingleConversion

There are quite a few others available in the Example Selector within CubeMX for the G0 series.

If you feel a post has answered your question, please click "Accept as Solution".
meena
Associate III

these examples i tried as a result reading same values for all channels