cancel
Showing results for 
Search instead for 
Did you mean: 

ADC measurements in sleep

FErma
Associate II

Hello everyone,

For one of our commercial product we are using STM32F0 as mcu, and IAR as compiler.

Since the device is battery powered, it sleeps for 1 sec then wakes up and does some adc measurements and sleeps for next 1 sec.

Instead of doing measurements at awake state, I want to measure adc channels at sleep state such that DMA shall measure adc channel every 100ms and store it in sram. For total 1 sec, I shall have 10 measurements. When mcu wakes up, I will take avarage of these 10 measurements and use it for further process. Is it possible to do that? If yes, how can I do it?

Thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User

Run a timer which will trigger ADC conversion every 100ms.

JW